AXIS#.SM.DEC

Description

Sets the deceleration ramp for service motion if set to greater than 0.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

See Acceleration Units for details.

Range

Depends on units. See Acceleration Units for details.

Default Value

30,000 rpm/s

Depends on units. See Acceleration Units for details.

Data Type

Float

See Also

Service Motion
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
AXIS1.SM.DEC

500eh

09h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.SM.DEC

510eh

09h

Unsigned32

Acceleration

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.SM.DEC

6409

1909

Unsigned32

Read/Write

Acceleration

AXIS2.SM.DEC

71945

1190

Unsigned32

Read/Write

Acceleration

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.SM.DEC

6409

Float

Read/Write

Acceleration